# emios_simple_pwm

## Overview

The eMIOS project is a simple demonstration example of the SDK eMIOS driver to use eMIOS as PWM generator.  
It configures eMIOS UC (Unified channel) as Output PWM Buffered (OPWMB) mode and generate one 10kHz, 25% duty cycle PWM.

## Supported Boards

````{container} board-selector

```{container} board-setup
:name: board-frdmmcxe31b

##### FRDM-MCXE31B

##### Hardware requirements
- Micro USB cable
- FRDM-MCXE31B Board
- Personal Computer
- Oscilloscope

##### Board settings
Probe the PWM signal using an oscilloscope
 - At J3-15 for PWM channel 0

##### Prepare the Demo
1.  Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board. 
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, following information can be seen on the OpenSDA terminal:

~~~~~~~~~~~~~~~~~~~~~
eMIOS simple PWM Example
~~~~~~~~~~~~~~~~~~~~~

```

```{container} board-setup
:name: board-frdmmcxe32b

##### FRDM-MCXE32B

##### Hardware requirements
- Micro USB cable
- FRDM-MCXE32B board
- Personal Computer
- Oscilloscope

##### Board settings
Probe the PWM signal using an oscilloscope
 - At J3-15 for PWM channel 0

##### Prepare the Demo
1.  Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board. 
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, following information can be seen on the OpenSDA terminal:

~~~~~~~~~~~~~~~~~~~~~
eMIOS simple PWM Example
~~~~~~~~~~~~~~~~~~~~~

```

````