# pwt_example

## Overview
The PWT project is a simple demonstration program of the SDK PWT driver. It sets up the PWT
hardware block to edge detection, capture control part and detects measurement trigger edges and
controls when and which pulse width register(s) will be updated. Once the input signal is received,
this example will print overflow flag status, positive pulse width and negative pulse width.

## Supported Boards

````{container} board-selector

```{container} board-setup
:name: board-frdmke15z

##### FRDM-KE15Z

##### Hardware requirements
- Micro USB cable
- FRDM-KE15Z board
- Personal Computer

##### Board settings
Connect input signal to J2-15

##### Prepare the Demo
1.  Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
2.  Open a serial terminal with the following settings:
   - 115200 baud rate
   - 8 data bits
   - No parity
   - One stop bit
   - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, the following message is displayed in the terminal:

~~~~~~~~~~~~

PWT example: input signal whose pulse width needs to be measured


Toggled Low overflow


Positive pulse width=16 usec


Negative pulse width=11 usec


Toggled High overflow


Positive pulse width=11 usec


Negative pulse width=17 usec

~~~~~~~~~~~~

```

```{container} board-setup
:name: board-frdmke16z

##### FRDM-KE16Z

##### Hardware requirements
- Micro USB cable
- FRDM-KE16Z board
- Personal Computer

##### Board settings
Connect input signal to J2-15

##### Prepare the Demo
1.  Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
2.  Open a serial terminal with the following settings:
   - 115200 baud rate
   - 8 data bits
   - No parity
   - One stop bit
   - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, the following message is displayed in the terminal:

~~~~~~~~~~~~

PWT example: input signal whose pulse width needs to be measured


Toggled Low overflow


Positive pulse width=16 usec


Negative pulse width=11 usec


Toggled High overflow


Positive pulse width=11 usec


Negative pulse width=17 usec

~~~~~~~~~~~~

```

```{container} board-setup
:name: board-frdmke17z

##### FRDM-KE17Z

##### Hardware requirements
- Micro USB cable
- FRDM-KE17Z board
- Personal Computer

##### Board settings
Connect input signal to J2-2

##### Prepare the Demo
1.  Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
2.  Open a serial terminal with the following settings:
   - 115200 baud rate
   - 8 data bits
   - No parity
   - One stop bit
   - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, the following message is displayed in the terminal:

~~~~~~~~~~~~

PWT example: input signal whose pulse width needs to be measured


Toggled Low overflow


Positive pulse width=16 usec


Negative pulse width=11 usec


Toggled High overflow


Positive pulse width=11 usec


Negative pulse width=17 usec

~~~~~~~~~~~~

```

```{container} board-setup
:name: board-frdmke17z512

##### FRDM-KE17Z512

##### Hardware requirements
- Micro USB cable
- FRDM-KE17Z512 board
- Personal Computer

##### Board settings
Connect input signal to J2-11

##### Prepare the Demo
1.  Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
2.  Open a serial terminal with the following settings:
   - 115200 baud rate
   - 8 data bits
   - No parity
   - One stop bit
   - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, the following message is displayed in the terminal:

~~~~~~~~~~~~

PWT example: input signal whose pulse width needs to be measured


Toggled Low overflow


Positive pulse width=16 usec


Negative pulse width=11 usec


Toggled High overflow


Positive pulse width=11 usec


Negative pulse width=17 usec

~~~~~~~~~~~~

```

```{container} board-setup
:name: board-frdmmcxc353

##### FRDM-MCXC353

##### Hardware requirements
- Micro USB cable
- FRDM-MCXC353 board
- Personal Computer

##### Board settings
Connect input signal to J2-7

##### Prepare the Demo
1.  Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
2.  Open a serial terminal with the following settings:
   - 115200 baud rate
   - 8 data bits
   - No parity
   - One stop bit
   - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, the following message is displayed in the terminal:

~~~~~~~~~~~~

PWT example: input signal whose pulse width needs to be measured


Toggled Low overflow


Positive pulse width=16 usec


Negative pulse width=11 usec


Toggled High overflow


Positive pulse width=11 usec


Negative pulse width=17 usec

~~~~~~~~~~~~

```

````