# Changelog Multicore Manager

All notable changes to this project will be documented in this file.

The format is based on [Keep a Changelog](https://keepachangelog.com/en/1.1.0/),
and this project adheres to [Semantic Versioning](https://semver.org/spec/v2.0.0.html).

## [Unreleased]

### Fixed

- MCUX-91737: On MU-based platforms (i.MX RT1160, RT1170, RT1180, RT700, K32L3A6, KW43B43, MCXW70, MCXL20, MCXE32B), MCMGR_TriggerEventForce() no longer overwrites an event the remote core has not read yet. Such an event is now queued and sent from the MU TX empty interrupt in the order of the calls, so an application event followed by an RPMsg-Lite notification is no longer lost. RPMsg-Lite doorbells identical to one already waiting are merged; other forced events are never merged and return kStatus_MCMGR_Error when their queue is full. The blocking MCMGR_TriggerEvent() now checks and writes the MU TX register with interrupts disabled, is sent after forced events queued before it, and returns kStatus_MCMGR_Error when MCMGR_BUSY_POLL_COUNT expires. Queued events are dropped on MCMGR_Init() and when the remote core is reset.

### Added

- Kconfig MCMGR_MU_FORCED_QUEUE_SIZE (forced events that can wait per MU, default 2, 3 on KW43B43 and MCXW70) and MCMGR_MU_RPMSG_DOORBELL_SLOTS (distinct RPMsg-Lite doorbells that can wait per MU, default 2, 8 on i.MX RT700). Both can also be set with a compiler definition.

## [v5.3.0]

### Added

- Added MCXE32B (dual Cortex-M7) porting layer.
- Remove obsolete unused platform layers
- Added initialization guard to public MCMGR API functions (RPSDK-1183): guarded functions return kStatus_MCMGR_NotReady before MCMGR_Init() completes.

### Fixed

- MCUX-88924: Fix KW43 ICS init-handshake hang (RPSDK-1183 regression): s_mcmgrInitialized is now set before mcmgr_platform_init_internal() enables the MU RX IRQ, so re-entrant ISR dispatch during MCMGR_Init() is no longer silently dropped by MCMGR_CHECK_INIT().
- MCUX-89876: Fix Coverity DEADCODE and UNUSED_VALUE findings in mcmgr_internal_core_api_imxrt700.c: align mcmgr_mu_channel_handler event-range guard with positive-logic form (matching imxrt1170), and aggregate mcmgr_trigger_event_internal return values in mcmgr_platform_init_internal_early so earlier errors are not silently overwritten.

## [v5.2.0]

### Changed

- Merged internal platform initialization into a single `mcmgr_platform_init_internal()` function.
- Simplified initialization API: `MCMGR_Init()` now handles both early and standard initialization internally.

### Deprecated

- `MCMGR_EarlyInit()` is now deprecated and a no-op. It remains for backward compatibility and may be removed in a future major version. Replace calls to `MCMGR_EarlyInit()` + `MCMGR_Init()` with a single `MCMGR_Init()` call.

### Migration Guide

**Before:**
```c
MCMGR_EarlyInit();
// ...
MCMGR_Init();
```

**After:**
```c
MCMGR_Init();
```

## [v5.1.0]

### Added

- Added mcxl14x parts support
- Added mcxw70 parts support
- Add new config `MCMGR_REMOTE_APP_EVENT_COUNT` for configurable remote application event count. This will expand number of application events available for MCMGR users. kMCMGR_RemoteApplicationEvent, kMCMGR_RemoteApplicationEvent1 .. kMCMGR_RemoteApplicationEvent4.
- Align Kinetis parts porting to changed register map

### Fixed

- Fix MISRA C-2012 Rule 20.8 violations.

## [v5.0.2]

### Added

- Added gcov options and configs to support mcmgr code coverage
- Added new test_weak_mu_isr testcase for devices with MU peripheral
- Added new test_heartbeat testcase showing heartbeat mechanism between primary and secondary cores using the MCMGR

## [v5.0.1]

### Added

- Added frdmimxrt1186 unit testing

### Changed

- [KW43] Rename core#1 reset control register

### Fixed

- Added CX flag into CMakeLists.txt to allow c++ build compatibility.
- Fix path to mcmgr headers directory in doxyfile

## [v5.0.0]

### Added

- Added `MCMGR_BUSY_POLL_COUNT` macro to prevent infinite polling loops in MCMGR operations.
- Implemented timeout mechanism for all polling loops in MCMGR code.
- Added support to handle more then two cores. Breaking API change by adding parameter `coreNum` specifying core number in functions bellow.

  * MCMGR_GetStartupData(uint32_t *startupData, mcmgr_core_t coreNum)
  * MCMGR_TriggerEvent(mcmgr_event_type_t type, uint16_t eventData, mcmgr_core_t coreNum)
  * MCMGR_TriggerEventForce(mcmgr_event_type_t type, uint16_t eventData, mcmgr_core_t coreNum)
  * typedef void (*mcmgr_event_callback_t)(uint16_t data, void *context, mcmgr_core_t coreNum);

  When registering the event with function `MCMGR_RegisterEvent()` user now needs to
  provide `callbackData` pointer to array of elements per every core in system (see README.md for example).In case of systems with only two cores the `coreNum` in callback can be ignored as events can arrive only from one core.
  Please see Porting guide for more details: [PortingGuideTo_v5.md](doxygen/porting_guide_to_v5.md)
- Updated all porting files to support new MCMGR API.
- Added new platform specific include file `mcmgr_platform.h`.
  It will contain common platform specific macros that can be then used in `mcmgr` and application.
  e.g. platform core count `MCMGR_CORECOUNT 4`.
- Move all header files to new `inc` directory.
- Added new platform-specific include files `inc/platform/<platform_name>/mcmgr_platform.h`.

### Added

- Add MCXL20 porting layer and unit testing

## [v4.1.7]

### Fixed

- `mcmgr_stop_core_internal()` function now returns `kStatus_MCMGR_NotImplemented` status code instead
  of `kStatus_MCMGR_Success` when device does not support stop of secondary core.
  Ports affected: `kw32w1`, `kw45b41`, `kw45b42`, `mcxw716`, `mcxw727`.

## [v4.1.6]

### Added

- Multicore Manager moved to standalone repository.
- Add porting layers for imxrt700, mcmxw727, kw47b42.
- New MCMGR_ProcessDeferredRxIsr() API added.

## [v4.1.5]

### Added

- Add notification into MCMGR_EarlyInit and mcmgr_early_init_internal functions to avoid using uninitialized data in their implementations.

## [v4.1.4]

### Fixed

- Avoid calling tx isr callbacks when respective Messaging Unit Transmit Interrupt Enable flag is not set in the CR/TCR register.
- Messaging Unit RX and status registers are cleared after the initialization.

## [v4.1.3]

### Added

- Add porting layers for imxrt1180.

### Fixed

- mu_isr() updated to avoid calling tx isr callbacks when respective Transmit Interrupt Enable flag is not set in the CR/TCR register.
- mcmgr_mu_internal.c code adaptation to new supported SoCs.

## [v4.1.2]

### Fixed

- Update mcmgr_stop_core_internal() implementations to set core state to kMCMGR_ResetCoreState.

## [v4.1.0]

### Fixed

- Code adjustments to address MISRA C-2012 Rules

## [v4.0.3]

### Fixed

- Documentation updated to describe handshaking in a graphic form.
- Minor code adjustments based on static analysis tool findings

## [v4.0.2]

### Fixed

- Align porting layers to the updated MCUXpressoSDK feature files.

## [v4.0.1]

### Fixed

- Code formatting, removed unused code

## [v4.0.0]

### Added

- Add new MCMGR_TriggerEventForce() API.

## [v3.0.0]

### Removed

- Removed MCMGR_LoadApp(), MCMGR_MapAddress() and MCMGR_SignalReady()

### Modified

- Modified MCMGR_GetStartupData()

### Added

- Added MCMGR_EarlyInit(), MCMGR_RegisterEvent() and MCMGR_TriggerEvent()
- Added the ability for remote core monitoring and event handling

## [v2.0.1]

### Fixed

- Updated to be Misra compliant.

## [v2.0.0]

### Added

- Support for lpcxpresso54114 board.

## [v1.1.0]

### Fixed

- Ported to KSDK 2.0.0.

## [v1.0.0]

### Added

- Initial release.

[Unreleased]: https://github.com/nxp-mcuxpresso/mcux-mcmgr/compare/v5.3.0...HEAD
[v5.3.0]: https://github.com/nxp-mcuxpresso/mcux-mcmgr/compare/v5.2.0...v5.3.0
[v5.2.0]: https://github.com/nxp-mcuxpresso/mcux-mcmgr/compare/v5.1.0...v5.2.0
[v5.1.0]: https://github.com/nxp-mcuxpresso/mcux-mcmgr/compare/v5.0.2...v5.1.0
[v5.0.2]: https://github.com/nxp-mcuxpresso/mcux-mcmgr/compare/v5.0.1...v5.0.2
[v5.0.1]: https://github.com/nxp-mcuxpresso/mcux-mcmgr/compare/v5.0.0...v5.0.1
[v5.0.0]: https://github.com/nxp-mcuxpresso/mcux-mcmgr/compare/v4.1.7...v5.0.0
[v4.1.7]: https://github.com/nxp-mcuxpresso/mcux-mcmgr/compare/v4.1.6...v4.1.7