MCUXpresso SDK Documentation

Note when debugging with JTAG mode

Note when debugging with JTAG mode#

When debugging with JTAG mode, the JTAG_MOD pin on MIMXRT1040-EVK board is reused. If the M.2 device is plugged in, the JTAG_MOD pin is pulled higher, resulting in debug failure. If this happens, ensure that the J80 Jumper is in the open state.