MCUXpresso SDK Documentation

How to add or remove boot header for XIP targets

How to add or remove boot header for XIP targets#

The MCUXpresso SDK for i.MX provides flexspi_nor_debug and flexspi_nor_release targets for each example and/or demo which supports XIP (eXecute-In-Place). These two targets add XIP_BOOT_HEADER to the image by default. Because of this, ROM can boot and run this image directly on external flash.

Macros for the boot leader:

Where to change the macros for each toolchain in MCUXpresso SDK?

Take hello_world as an example:

  • IAR

  • MDK

  • ARMGCC

    Change the configuration in CMakeLists.txt.

  • MCUX