MCUXpresso SDK DSP Enablement
The DSP-specific enablement is available inside the MCUXpresso SDK release package for RT500. The path is: <SDK_ROOT>/devices/MIMXRT595S/
Unified device and peripheral driver source code that compiled for both ARM and DSP cores.
Note: Only a limited subset of peripheral drivers and components are supported on the DSP.
<SDK_ROOT>/boards/evkmimxrt595/dsp_examples/
DSP example applications are available at:<SDK_ROOT>/middleware/multicore/rpmsg_lite/
Unified RPMsg-Lite multicore communication library, with porting layers for ARM and DSP cores. <SDK_ROOT>/middleware/dsp/audio_framework/
Xtensa Audio Framework (XAF) for DSP core
Parent topic:Install MCUXpresso SDK