MCUXpresso SDK Documentation

Build an example application

Build an example application#

To build an example application, perform the following steps.

  1. Drag and drop the SDK zip file into the Installed SDKs view to install an SDK.

    In the window that appears, click OKand wait until the import has finished.

  2. On the Quickstart Panel, click Import SDK example(s).

  3. In the window that appears, select mimxrt700evk or kits and click Next.

  4. Expand the demo_apps folder and select hello_world_demo_cm33_core0. Then, click Next.

  5. Click Finish.

Parent topic:Run a demo using MCUXpresso IDE