MCUXpresso SDK release package
The MCUXpresso DSC SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, devices, documentation, and middleware.
Device support
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Parent topic:Device support
Demo application and other examples
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
Parent topic:Device support
Parent topic:MCUXpresso SDK release package
CMSIS DSP Lib
CMSIS DSP Library
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
Parent topic:CMSIS DSP Lib
Parent topic:MCUXpresso SDK release package
Operating system
FreeRTOS
The MCUXpresso SDK is integrated with FreeRTOS OS.
Parent topic:Operating system
Parent topic:MCUXpresso SDK release package
Middleware
Multicore
Multicore Software Development Kit
Parent topic:Middleware
Parent topic:MCUXpresso SDK release package