Getting Started with MCUXpresso for EVK-MIMX8MNDDR3L# Table of Contents Overview MCUXpresso SDK board support folders Example application structure Locating example application source files Toolchain introduction Compiler/Debugger Run a demo application using IAR Build an example application Run an example application Run a demo using ARMGCC / VSCODE Running an application by U-Boot Run a flash target demo by UUU Set up environment Download the MfgTool Switch to Download Mode Build an example application Run an example application How to determine COM port How to define IRQ handler in CPP files