MCUXpresso SDK Documentation

MISRA compliance

MISRA compliance#

All MCUXpresso SDK drivers comply to MISRA 2012 rules with exceptions in Table 1.

|Exception rules

|Description

| |—————–|————-| |Directive 4.4

|Sections of code should not be commented out.

| |Directive 4.5

|Identifiers in the same name space with overlapping visibility should be typographically unambiguous.

| |Directive 4.6

|Typedefs that indicate size and signedness should be used in place of the basic numerical types.

| |Directive 4.8

|If a pointer to a structure or union is never dereferenced within a translation unit, then the implementation of the object should be hidden.

| |Directive 4.9

|A function should be used in preference to a function-like macro where they are interchangeable.

| |Directive 4.13

|Functions which are designed to provide operations on a resource should be called in an appropriate sequence.

| |Rule 1.2

|Language extensions should not be used.

| |Rule 2.3

|A project should not contain unused type declarations.

| |Rule 2.4

|A project should not contain unused tag declarations.

| |Rule 2.5

|A project should not contain unused macro declarations.

| |Rule 2.6

|A function should not contain unused label declarations.

| |Rule 2.7

|There should be no unused parameters in functions.

| |Rule 4.2

|Trigraphs should not be used.

| |Rule 5.1

|External identifiers shall be distinct.

| |Rule 5.4

|Macro identifiers shall be distinct.

| |Rule 5.9

|Identifiers that define objects or functions with internal linkage should be unique.

| |Rule 8.7

|Functions and objects should not be defined with external linkage if they are referenced in only one translation unit.

| |Rule 8.9

|An object should be defined at block scope if its identifier only appears in a single function.

| |Rule 8.11

|When an array with external linkage is declared, its size should be explicitly specified.

| |Rule 8.13

|A pointer should point to a const-qualified type whenever possible.

| |Rule 10.5

|The value of an expression should not be cast to an inappropriate essential type.

| |Rule 11.4

|A conversion should not be performed between a pointer to object and an integer type.

| |Rule 11.5

|A conversion should not be performed from pointer to void into pointer to object.

| |Rule 12.1

|The precedence of operators within expressions should be made explicit.

| |Rule 12.3

|The comma operator should not be used.

| |Rule 12.4

|Evaluation of constant expressions should not lead to unsigned integer wrap-around.

| |Rule 13.3

|A full expression containing an increment (++) or decrement (–) operator should have no other potential side effects other than that caused by the increment or decrement operator.

| |Rule 15.4

|There should be no more than one break or go to statement used to terminate any iteration statement.

| |Rule 17.5

|The function argument corresponding to a parameter declared to have an array type shall have an appropriate number of elements.

| |Rule 17.8

|A function parameter should not be modified.

| |Rule 19.2

|The union keyword should not be used.

| |Rule 20.1

|#include directives should only be preceded by preprocessor directives or comments.

| |Rule 20.10

|The # and ## preprocessor operators should not be used.

| |Rule 21.1

|#define and #undef shall not be used on a reserved identifier or reserved macro name.

| |Rule 21.2

|A reserved identifier or macro name shall not be declared.

| |Rule 21.12

|The exception handling features of <fenv.h> should not be used.

|