Soc Arch, Device, Board and Shield Definition
Soc Arch
MCUXpresso SDK supports all mainstream soc architectures like ARM, RISCV, DSP, etc. The soc architecture specific data are recorded in mcuxsdk/arch/<arch> folder.
Here is the hierarchy of arch folder:
arch:
arm:
CMSIS: CMSIS headers
configuration: Commonly shared build configuration data
cortexm: Core settings
target: Commonly shared build targets data like debug and release
dsp56800:
riscv:
xtensa:
Board
Board data stays in examples/_boards folder. Here is a hierarchy demonstrate with single core device board frdmk22f and multicore device board evkbmimxrt1170:
_boards:
frdmk22f: # A single core device board
board.c: Board common configuration
board.h:
clock_config.c: clock configuraion
clock_config.h:
CMakeLists.txt: Board specific contents including components and configuration
Kconfig: Board Kconfig, mainly specify board specific component and project segment dependency
Kconfig.defconfig: Board specific components selection and configuration for invisible Kconfig symbols
prj.conf: Board specific components selection and configuration
board.yml: Board hardware data like on flash memory, optional
example.yml: The supported toolchains and build configuration targets
IDE.yml: IDE flash and debug related settings for GUI and standalone project generation
variable.cmake: Board variables
board_runner.cmake: Board debug settings
demo_apps:
prj.conf: components selection and configuration by all demo_apps, optional
hello_world:
reconfig.cmake: Board example reconfig, mainly replace, remove some default board settings
prj.conf: Board example specific component selection and configuration
reconfig.cmake: Board example category reconfig, mainly replace, remove some default settings
prj.conf: Board example category specific component selection and configuration
rtos_examples: # like above demo_apps
freertos_hello:
reconfig.cmake:
prj.conf:
reconfig.cmake:
prj.conf:
evkbmimxrt1170: # A multicore device board
board.c: Board common configuration
board.h:
clock_config.c: clock configuraion
clock_config.h:
dcd.c: device configuration data
dcd.h:
display_support.c: display configuration
display_support.h:
cm4: # Core specific contents folder
example.yml: Board core specific example list
IDE.yml: Board core specific IDE flash and debug related settings for GUI and standalone project generation
Kconfig: Board core software Kconfig, mainly specify board core specific component and project segment dependency
Kconfig.defconfig: Board core specific components selection and configuration for invisible Kconfig symbols
prj.conf: Board core specific components selection and configuration
setting.cmake: Board core specific data and settings
variable.cmake: Board core specific variables
cm7: # Just like above cm4 core
example.yml:
IDE.yml:
Kconfig:
Kconfig.defconfig:
prj.conf:
setting.cmake:
variable.cmake:
CMakeLists.txt: Board specific contents like components and settings
Kconfig: Board software Kconfig, mainly specify board specific component and project segment dependency
Kconfig.defconfig: Board specific components selection and configuration for invisible Kconfig symbols
prj.conf: Board specific components selection and configuration
board.yml: Board hardware data like on flash memory, optional
variable.cmake: Board variables
board_runner.cmake: Board debug settings
demo_apps:
prj.conf: components selection and configuration by all demo_apps, optional
reconfig.cmake: Board example category reconfig, mainly replace, remove some default board settings
hello_world:
cm4:
reconfig.cmake: Board core specific example reconfig, mainly replace, remove some default board settings
prj.conf: Board core example specific components selection and configuration
cm7:
reconfig.cmake:
prj.conf:
reconfig.cmake: Board example category reconfig, mainly replace, remove some default board settings
prj.conf: Board example category specific component selection and configuration
The board level supported toolchains and build configuration targets shall be recorded in the example.yml. A typical board example.yml is like
board.toolchains:
- +armgcc@debug
- +armgcc@release
- +iar@debug
- +iar@release
- +mdk@debug
- +mdk@release
All examples under the board share the toolchains and targets in the board example.yml.
Shield
Shield is an addon which is attached to a board to extend its features and functionalities. All shields folder are put under its mother board folder. The structure is like
_boards:
<board>:
shields:
<shield>:
<example category>:
CMakeLists.txt:
Kconfig:
prj.conf:
<other_shield>:
<example category>:
CMakeLists.txt:
Kconfig:
prj.conf:
The shield shares the board example.yml for toolchains and targets support. The shield CMakelists.txt shall be added into the board CMakeLists.txt with mcux_add_cmakelists and the shield Kconfig shall be rsource in the board Kconfig.
Device
Data
Device data stays in devices folder. Here is the device data hierarchy demonstrated with single core device MK22F51212 and multicore device MIMXRT1176
devices:
Kinetis: Device socs sery
MK22F25612:
Kconfig: Device Kconfig, mainly specify device specific component and project segment dependency
Kconfig.chip: Device hardware Kconfig related to device and core
Kconfig.defconfig: Device specific components selection and configuration for invisible Kconfig symbols
CMakeLists.txt: Device specific contents like components and settings, usually, just load mainset cmakelist
driver:
CMakeLists.txt: Device specific drivers
Kconfig: Device specific drivers Kconfig
prj.conf: Device specific components selection and configuration for visible Kconfig symbols
MK22F51212:
Kconfig: Device software Kconfig, mainly specify device specific component and project segment dependency
Kconfig.chip: Device hardware Kconfig related to device and core
Kconfig.defconfig: Device specific components selection and configuration for invisible Kconfig symbols
CMakeLists.txt: Device specific contents like components and settings
driver:
CMakeLists.txt: Device specific drivers
Kconfig: Device specific drivers Kconfig
prj.conf: Device specific components selection and configuration
prj.conf: Components selection and configuration by all Kinetis series
RT:
MIMXRT1175:
cm4:
driver:
CMakeLists.txt: Device core specific drivers
Kconfig: Device core specific drivers Kconfig
Kconfig: Device core software Kconfig, mainly specify device specific component and project segment dependency
Kconfig.chip: Device core hardware Kconfig related to device and core
Kconfig.defconfig: Device core specific components selection and configuration for invisible Kconfig symbols
setting.cmake: Device core specific data and settings
variable.cmake: Device core specific variables
prj.conf: Device core specific components selection and configuration
cm7: # just like core cm4
driver:
CMakeLists.txt:
Kconfig:
Kconfig:
Kconfig.chip:
Kconfig.defconfig:
setting.cmake:
variable.cmake:
prj.conf:
CMakeLists.txt: Device specific contents like components and settings, usually, just load mainset cmakelist
driver:
CMakeLists.txt: Device specific drivers
Kconfig: Device specific drivers Kconfig
Kconfig: Device
Kconfig.chip: Device software Kconfig, mainly specify board specific component and project segment dependency
Kconfig.defconfig: Device specific components selection and configuration for invisible Kconfig symbols
prj.conf: Device specific components selection and configuration
MIMXRT1176:
cm4:
driver:
CMakeLists.txt: Device core specific drivers
Kconfig: Device specific drivers Kconfig
Kconfig: Device core software Kconfig, mainly specify board specific component and project segment dependency
Kconfig.chip: Device core hardware Kconfig related to device and core
Kconfig.defconfig: Device core specific components selection and configuration for invisible Kconfig symbols
setting.cmake: Device core specific data and settings
variable.cmake: Device core specific variables
prj.conf: Device core specific components selection and configuration
cm7: # just like core cm4
driver:
CMakeLists.txt:
Kconfig:
Kconfig:
Kconfig.chip:
Kconfig.defconfig:
setting.cmake:
variable.cmake:
prj.conf:
CMakeLists.txt: Device specific contents like components and settings
driver:
CMakeLists.txt: Device specific drivers
Kconfig: Device specific drivers Kconfig
Kconfig: Device
Kconfig.chip: Device software Kconfig, mainly specify board specific component and project segment dependency
Kconfig.defconfig: Device specific components selection and configuration for invisible Kconfig symbols
prj.conf: Device specific components selection and configuration
prj.conf: Components selection and configuration by all RT series
prj.conf: Components selection and configuration by all devices
Switch a Device For a Board Example Build
The device dedicated startup, linker, system, feature files are recorded in cmake files with variables defined in the device Kconfig.chip. Here is the typical device_header.cmake for system and startup:
# device spcific drivers for single core device
if(CONFIG_MCUX_COMPONENT_device.CMSIS)
mcux_add_source(BASE_PATH ${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${device} SOURCES fsl_device_registers.h
"${CONFIG_MCUX_HW_DEVICE_CORE}.h" "${CONFIG_MCUX_HW_DEVICE_CORE}_features.h" "${CONFIG_MCUX_HW_DEVICE_CORE}_COMMON.h" "../${soc_periph}/*.h")
mcux_add_include(BASE_PATH ${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${device} INCLUDES .)
mcux_add_include(BASE_PATH ${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${soc_periph} INCLUDES .)
endif()
if(CONFIG_MCUX_COMPONENT_device.system)
mcux_add_source(BASE_PATH ${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${device} SOURCES system_${CONFIG_MCUX_HW_DEVICE_CORE}.c
system_${CONFIG_MCUX_HW_DEVICE_CORE}.h)
mcux_add_include(BASE_PATH ${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${device} INCLUDES .)
endif()
if(CONFIG_MCUX_COMPONENT_device.startup)
mcux_add_source(
BASE_PATH
${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${device}
SOURCES
iar/startup_${CONFIG_MCUX_HW_DEVICE_CORE}.s
TOOLCHAINS
iar
CONFIG
true)
mcux_add_source(
BASE_PATH
${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${device}
SOURCES
gcc/startup_${CONFIG_MCUX_HW_DEVICE_CORE}.S
TOOLCHAINS
armgcc
CONFIG
true)
mcux_add_source(
BASE_PATH
${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${device}
SOURCES
arm/startup_${CONFIG_MCUX_HW_DEVICE_CORE}.S
TOOLCHAINS
mdk
CONFIG
true)
endif()
Here is the Kconfig.chip for MK22F51212:
config MCUX_HW_CORE
string
default "cm4f"
config MCUX_HW_CORE_CM4F
bool
default y
config MCUX_HW_CORE_ID
string
default "core0"
config MCUX_HW_CORE_ID_CORE0
bool
default y
config MCUX_HW_DEVICE_CORE
string
default "MK22F51212"
config MCUX_HW_FPU
string
default "SP_FPU"
config MCUX_HW_FPU_TYPE
string
default "fpv4_sp"
config MCUX_HW_FPV4_SP
bool
default y
config MCUX_HW_INT_PRIO_BITS
int
default 4
config MCUX_HW_SOC_SERIES_KINETIS
bool
default y
config MCUX_HW_SOC_SINGLECORE_DEVICE
bool
default y
# device related
config MCUX_HW_DEVICE_ID_MK22FN512xxx12
bool
choice MCUX_HW_DEVICE_PART_MK22F51212
prompt "Device MK22F51212 Part"
config MCUX_HW_DEVICE_PART_MK22FN512VDC12
bool "MK22FN512VDC12"
select MCUX_HW_DEVICE_ID_MK22FN512xxx12
config MCUX_HW_DEVICE_PART_MK22FN512VLL12
bool "MK22FN512VLL12"
select MCUX_HW_DEVICE_ID_MK22FN512xxx12
config MCUX_HW_DEVICE_PART_MK22FN512VLH12
bool "MK22FN512VLH12"
select MCUX_HW_DEVICE_ID_MK22FN512xxx12
config MCUX_HW_DEVICE_PART_MK22FN512VFX12
bool "MK22FN512VFX12"
select MCUX_HW_DEVICE_ID_MK22FN512xxx12
config MCUX_HW_DEVICE_PART_MK22FN512CAP12
bool "MK22FN512CAP12"
select MCUX_HW_DEVICE_ID_MK22FN512xxx12
config MCUX_HW_DEVICE_PART_MK22FN512VMP12
bool "MK22FN512VMP12"
select MCUX_HW_DEVICE_ID_MK22FN512xxx12
endchoice
config MCUX_HW_DEVICE_ID
string
default "MK22FN512xxx12" if MCUX_HW_DEVICE_ID_MK22FN512xxx12
config MCUX_HW_DEVICE_PART
string
default "MK22FN512VDC12" if MCUX_HW_DEVICE_PART_MK22FN512VDC12
default "MK22FN512VLL12" if MCUX_HW_DEVICE_PART_MK22FN512VLL12
default "MK22FN512VLH12" if MCUX_HW_DEVICE_PART_MK22FN512VLH12
default "MK22FN512VFX12" if MCUX_HW_DEVICE_PART_MK22FN512VFX12
default "MK22FN512CAP12" if MCUX_HW_DEVICE_PART_MK22FN512CAP12
default "MK22FN512VMP12" if MCUX_HW_DEVICE_PART_MK22FN512VMP12
# For chipmodel generated files
config MCUX_TOOLCHAIN_LINKER_DEVICE_PREFIX
string
default "MK22FN512xxx12" if MCUX_HW_DEVICE_ID_MK22FN512xxx12
config MCUX_TOOLCHAIN_MCUX_STARTUP
string
default "mk22f51212"
# Toolchain related
config MCUX_TOOLCHAIN_IAR_CPU_IDENTIFIER
string
default "MK22FN512xxx12" if MCUX_HW_DEVICE_ID_MK22FN512xxx12
config MCUX_TOOLCHAIN_MDK_CPU_IDENTIFIER
string
default "MK22FN512VDC12" if MCUX_HW_DEVICE_PART_MK22FN512VDC12
default "MK22FN512VLL12" if MCUX_HW_DEVICE_PART_MK22FN512VLL12
default "MK22FN512VLH12" if MCUX_HW_DEVICE_PART_MK22FN512VLH12
default "MK22FN512VFX12" if MCUX_HW_DEVICE_PART_MK22FN512VFX12
default "MK22FN512CAP12" if MCUX_HW_DEVICE_PART_MK22FN512CAP12
default "MK22FN512VMP12" if MCUX_HW_DEVICE_PART_MK22FN512VMP12
config MCUX_TOOLCHAIN_JLINK_CPU_IDENTIFIER
string
default "MK22FN512xxx12"
In a build, when the device is set down, then the corresponding device cmake and Kconfig will be loaded, so that device dedicated linker, startup, system, feature files will get the correct variable name and involved into build.
So how a device is chosen for a board build?
For a typical board example build without designating the device:
west build -b frdmk22f examples/demo_apps/hello_world -p
The target device is set through the device in the board variable.cmake:
if (NOT DEFINED device)
mcux_set_variable(device MK22F51212) # default device is set in the board.cmake
endif()
include(${SdkRootDirPath}/devices/Kinetis/K/${device}/variable.cmake)
The default device is usually the main set of the device family. If you want to or need to try subset device, you can use --device argument, like
west build -b frdmk22f examples/demo_apps/hello_world --device MK22F12810
Then the MK22F12810 dedicated startup, linker, system and feature files will be used for this build.
Switch a Device Part For a Board Example Build
When the device is set down through cmake, you can use Kconfig to switch device part.
With the following cmd, you can start the Kconfig GUI:
west build -b frdmk22f examples/demo_apps/hello_world -t guiconfig -p
Then you can select different device part in the Kconfig, save it and west build.
Assembly Point
All the above data are pieces of building blocks. For any build process, all data shall be loaded for selection and configuration. The assembly point is the start entry from where all cmakes and Kconfigs can be loaded.
The assembly point for all cmakes is the root CMakeLists.txt. It looks like
# Load device CMakeLists.txt
mcux_add_cmakelists(${SdkRootDirPath}/${device_root}/${soc_portfolio}/${soc_series}/${device})
# Load board CMakeLists.txt
mcux_add_cmakelists(${SdkRootDirPath}/examples/)
# Load all drivers
mcux_load_all_cmakelists_in_directory(${SdkRootDirPath}/drivers)
# all components
mcux_add_cmakelists(${SdkRootDirPath}/components)
# middlewares
mcux_add_cmakelists(${SdkRootDirPath}/rtos/freertos/backoffalgorithm OPTIONAL)
mcux_add_cmakelists(${SdkRootDirPath}/rtos/freertos/corehttp OPTIONAL)
mcux_add_cmakelists(${SdkRootDirPath}/rtos/freertos/corejson OPTIONAL)
mcux_add_cmakelists(${SdkRootDirPath}/rtos/freertos/coremqtt OPTIONAL)
mcux_add_cmakelists(${SdkRootDirPath}/rtos/freertos/coremqtt-agent OPTIONAL)
mcux_add_cmakelists(${SdkRootDirPath}/rtos/freertos/corepkcs11 OPTIONAL)
mcux_add_cmakelists(${SdkRootDirPath}/rtos/freertos/freertos-kernel OPTIONAL)
mcux_add_cmakelists(${SdkRootDirPath}/middleware/usb OPTIONAL)
mcux_add_cmakelists(${SdkRootDirPath}/middleware/fatfs OPTIONAL)
mcux_add_cmakelists(${SdkRootDirPath}/middleware/littlefs OPTIONAL)
# ......
The assembly point for all Kconfig is the root Kconfg.mcuxpresso:
# board
rsource "examples/Kconfig"
# device
rsource "devices/Kconfig"
# Driver config
menu "Driver Configuration"
rsource "drivers/Kconfig"
osource "rtos/freertos/freertos-drivers/Kconfig"
endmenu
# Component config
rsource "components/Kconfig"
# middleware config
menu "Middleware"
osource "middleware/wifi_nxp/Kconfig"
osource "middleware/mbedtls/Kconfig"
osource "middleware/usb/Kconfig"
osource "middleware/fatfs/Kconfig"
osource "middleware/littlefs/Kconfig"
osource "middleware/multicore/Kconfig"
......
endmenu
# RTOS config
menu "RTOS"
menu "FreeRTOS"
osource "rtos/freertos/freertos-kernel/Kconfig"
osource "rtos/freertos/backoffalgorithm/Kconfig"
......
endmenu
endmenu
menu "External Modules"
osource "$(KCONFIG_BINARY_DIR)/Kconfig.modules"
endmenu
For any component, its cmake include and Kconfig rsource are generally aligned which means they shall stay together with each other.