Hardware requirements#
Micro USB cable
two MCIMX8ULP-EVK/EVK9 boards
J-Link Debug Probe
5V power supply
Personal Computer
Board settings#
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C0 pins of MASTER_BOARD are connected with LPI2C0 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
I2C0_SCL J20-10 I2C0_SCL J20-10
I2C0_SDA J20-9 I2C0_SDA J20-9
GND GND
Please note this application can’t support running with Linux BSP!
Prepare the Demo#
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board EDMA example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .