Hardware requirements#
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings#
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo#
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below.
LPI2C example -- Read Accelerometer Value
Found an FXOS8700 on board , the device address is 0x1e .
The accel values:
status_reg = 0x5 , x = 17156 , y = 22528 , z = -17600
status_reg = 0x5 , x = 16132 , y = 21760 , z = -17344
status_reg = 0x5 , x = 15108 , y = 21760 , z = -17344
status_reg = 0x5 , x = 16132 , y = 22272 , z = -18368
status_reg = 0x5 , x = 16132 , y = 23040 , z = -17344
status_reg = 0x5 , x = 16644 , y = 22272 , z = -16320
status_reg = 0x5 , x = 15364 , y = 23040 , z = -16576
status_reg = 0x5 , x = 16388 , y = 22528 , z = -17344
status_reg = 0x5 , x = 17412 , y = 21760 , z = -16832
status_reg = 0x5 , x = 16644 , y = 23296 , z = -15808
End of LPI2C example .