MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings#

  • CM33: Connect input signal to J11-3

  • note: square wave at fixed rate is recommended as the input signal for easily checking the result.

Prepare the Demo#

  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo#

When the example runs successfully, the following message is displayed in the terminal:

TPM dual-edge capture example

Once the input signal is received the input capture values are printed

The input signal's pulse width is calculated from the capture values & printed

Capture value C(n)V=8c40

Capture value C(n+1)V=e104

Input signals pulse width=904 us