Hardware requirements
Mini/micro USB cable
EVKB-IMXRT1050 board
Personal Computer
An encoder with PHASE A/B signals.
Board settings
For pin connection between board and encoder, J22.5 -> kXBARA1_InputIomuxXbarIn21 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J22.6 -> kXBARA1_InputIomuxXbarIn22 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB J22.3 -> kXBARA1_InputIomuxXbarIn23 -> kXBARA1_OutputEnc1Index -> ENC_INDEX
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
${ANCHOR}