Hardware requirements#
Mini/micro USB cable
Two EVK-MIMXRT1050 boards
Personal Computer
Board settings#
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J23-6 LPI2C1_SCL J23-6
LPI2C1_SDA J23-5 LPI2C1_SDA J23-5
GND J24-7 GND J24-7
Prepare the Demo#
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following message shows in the terminal if the example runs successfully.
LPI2C board2board EDMA example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
~~~~~~~~~~~~~~~~~~~~~