Hardware requirements#
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA USB on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
Consider special errata 005829 feature, the 1st valid MB should be used as reserved one. The TX MB number will change from 8 to 9, while RX MB number will change from 9 to 10 When the example runs successfully, following information can be seen on the OpenSDA terminal:
==FlexCAN loopback functional example -- Start.==
Send message from MB9 to MB10
tx word0 = 0x11223344
tx word1 = 0x55667788
Receved message from MB10
rx word0 = 0x11223344
rx word1 = 0x55667788
==FlexCAN loopback functional example -- Finish.==