Hardware requirements#
Mini/micro USB cable
MIMXRT1060-EVKC board
Personal Computer
USB to Com Converter
Board settings#
Connect pin:
RX of USB2COM to J16-2
TX of USB2COM to J16-1
GND of USB2COM to J16-7
Prepare the Demo#
Connect the USB2COM Converter to the host PC
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, the log would be seen on the UART Terminal port which connected to the USB2COM like:
FLEXIO UART RX ring buffer example
Send back received data
Echo every 8 bytes