MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • evkcmimxrt1060 board

  • Personal Computer

  • One of the following modules:

    • Embedded Artists 1XK M.2 Module (EAR00385) - direct M2 connection.

    • Embedded Artists 1ZM M.2 Module (EAR00364) - direct M2 connection.

    • Embedded Artists 2EL M.2 Module (Rev-A1) - direct M2 connection.

    • Embedded Artists 2LL M.2 Module (EAR00500) - direct M2 connection.

Board settings#

Before building the example application select Wi-Fi module macro in the edgefast_bluetooth_app.h. (see #define WIFI_BOARD). If you want to use Embedded Artists 1XK M.2 Module(EAR00385), please change the macro to WIFI_IW416_BOARD_MURATA_1XK_M2. If you want to use Embedded Artists 1ZM M.2 Module(EAR00364), please change the macro to WIFI_88W8987_BOARD_MURATA_1ZM_M2. If you want to use Embedded Artists 1ZM M.2 Module(Rev-A1), please change the macro to WIFI_IW612_BOARD_MURATA_2EL_M2. If you want to use Embedded Artists 2LL M.2 Module(EAR00500), please change the macro to WIFI_IW610_BOARD_MURATA_2LL_M2.

Jumper settings for RT1060-EVKC (enables external 5V supply):#

remove J40 5-6 connect J40 1-2 connect J45 with external power(controlled by SW6)

Murata Solution Board settings#

Embedded Artists 1XK module datasheet: https://www.embeddedartists.com/doc/ds/1XK_M2_Datasheet.pdf Embedded Artists 1ZM module datasheet: https://www.embeddedartists.com/doc/ds/1ZM_M2_Datasheet.pdf Embedded Artists 2EL module datasheet: https://www.embeddedartists.com/doc/ds/2EL_M2_Datasheet.pdf Embedded Artists 2LL module datasheet: https://www.embeddedartists.com/wp-content/uploads/2024/12/2LL_M2_Datasheet.pdf

The hardware should be reworked according to the Hardware Rework Guide for MIMXRT1060-EVKC and Murata M.2 Module in document Hardware Rework Guide for EdgeFast BT PAL.

Note: To ensure that the LITTLEFS flash region has been cleaned, all flash sectors need to be erased before downloading example code. After downloaded binary into qspiflash and boot from qspiflash directly, please reset the board by pressing SW7 or power off and on the board to run the application.