Hardware requirements#
Micro USB cable
two MCIMX7ULP-EVK boards
J-Link Debug Probe
5V power supply
Personal Computer
Board settings#
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C3 pins of MASTER_BOARD are connected with LPI2C3 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
I2C3_SCL TP24 I2C3_SCL TP24
I2C3_SDA TP26 I2C3_SDA TP26
GND GND
Please note this application can’t support running with Linux BSP!
Prepare the Demo#
Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
Connect a micro USB cable between the host PC and the J6 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
End of LPI2C example .