Hardware requirements#
Micro USB cable
MIMX8MN6-EVK board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings#
No special settings are required.
Please note this application can’t support booting by uboot! and accordingly it does not support Flash target! This example aims to show the basic usage of the IP’s function, some of the used Resources are assigned to Cortex-A core by uboot. To run the example, boot the A core into U-Boot and run the following command in the U-Boot console before starting the example to re-assign the resource.
u-boot=> mw.b 0x303d022c 1 1
Prepare the Demo#
Connect 12V power supply and J-Link Debug Probe to the board, switch SW101 to power on the board
Connect a USB cable between the host PC and the J901 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, the log would be seen on the debug terminal like:
USART CMSIS SDMA example
Board receives 8 characters then sends them out
Now please input: