Hardware requirements
Micro USB cable
EVK-MIMX8M Plus board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings
Use Oscilloscope to measure and observe the Test Point J21-32 output signal.
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW3 to power on the board
Connect a USB cable between the host PC and the J23 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
These instructions are displayed/shown on the terminal window:
PWM driver example.