MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • EVK-MIMX8M Plus board

  • J-Link Debug Probe

  • 12V power supply

  • Personal Computer

Board settings#

No special settings are required.

Please note this application can’t support running with Linux BSP!

Prepare the Demo#

  1. Connect 12V power supply and J-Link Debug Probe to the board, switch SW3 to power on the board

  2. Connect a USB cable between the host PC and the J23 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the example runs successfully, you will see the temperature output from the terminal when the pre-set threshold is reached.

NOTE: Average temperature threshold is 50 celsius degree by default, you can modify this value to facilitate testing the effect!