Hardware requirements#
Micro USB cable
MIMX8ULP-EVK/EVK9 board
RK055MHD091 MIPI panel
J-Link Debug Probe
5V power supply
Personal Computer
Board settings#
No special settings are required.
Note!
This case does not support ddr and flash target.
This case runs together with Linux.
Prepare the Demo#
Connect the RK055MHD091 MIPI panel onto EVK board.
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Turn on the power switch on your board to begin running the demo.
Running the demo#
When running the demo, the debug console shows the menu to command the CM33 to start the low power display. Before you input the command to run the low power display, please put the Linux into suspend (APD domain into Power Down mode) by command in the APD domain console: $echo mem > /sys/power/state After Linux goes into suspend mode, please input the āZā in RTD console to start low power display. The display panel will show fullscreen color, the color switch between RED/GREEN/BLUE every second.
AD entered Active mode
Start SRTM communication
Task 1 is working now
#################### Power Mode Switch Task ####################
Build Time: May 11 2023--16:54:05
Core Clock: 160000000Hz
Boot Type: Single Boot Type
Select the desired operation
Press Z for low power display.
Press M for switch Voltage Drive Mode between OD/ND/UD.
Waiting for power mode select..