MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • EVK-MIMXRT1015 board

  • Personal Computer

  • Oscilloscope

Board settings#

  • Connect input signal to J17-2.

  • Use oscilloscope to measure output the signal pin at J17-1.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo#

When the demo runs successfully, the following message is displayed in the terminal:


****Input capture example.****

****Provide a signal input to the QTMR pin****

Captured Period time = 1ms

****Output PWM example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~


Note:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
3. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
4. Start debugging in IDE.
   - Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.