MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

  • Headphone

Board settings#

Insert headphone to J101.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Press the reset button on your board to begin running the demo.

Running the demo#

When the demo runs successfully, you can hear the sound and the log would be seen on the OpenSDA terminal like:

PDM SAI multi channel edma example started!