Hardware requirements#
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output in the terminal window:
EdgeLock Enclave Sub-System crypto example:
****************** Load EdgeLock FW ***********************
EdgeLock FW loaded and authenticated successfully.
****************** Start RNG ******************************
EdgeLock RNG Start success.
EdgeLock RNG ready to use.
****************** Initialize EdgeLock services ***********
EdgeLock services initialized successfully.
****************** Open EdgeLock session ******************
Open session successfully. Session ID: 0xf623c27f
****************** Create Key Store ***********************
Open service and create Key Store successfully. Key Store ID: 0xf623ccff
****************** Key Management Open ********************
Open Key management service successfully. Key Handle ID: 0xf623ccb7
****************** Key Generate (AES ECB 128) *************
Key for AES-ECB generated successfully. Key ID: 0xcafe
****************** Open cipher service ********************
Open Cipher service successfully. Handle ID: 0xf623f7cf
****************** Cipher AES ECB *************************
Output size returned by AES-ECB encryption is : 0x20
AES-ECB crypto encryption and decryption using keys in ELE success.
****************** Key Generate (AEAD) ********************
Key for AES-GCM generated successfully. Key ID: 0x6fffffff
****************** Cipher AES AEAD (GCM) ******************
Output size returned by AES-AEAD encryption is : 0x30
AES-AEAD crypto encryption and decryption using keys in ELE success.
****************** Open MAC service ***********************
Open MAC service successfully. Handle ID: 0xf623f367
****************** Key Generate (HMAC_SHA256) *************
Key for HMAC_SHA256 generated successfully. Key ID: 0x6ffffffe
****************** HMAC_SHA256 ****************************
HMAC_SHA256 has been generated successfully
HMAC_SHA256 has been verified successfully
****************** Key Generate (ECC NIST P256) ***********
Key generated successfully. Key Pair ID: 0x6ffffffd
****************** Open Sign service **********************
Sign service open successfully. Signature generation handle ID: 0xf623f317
****************** ECC NIST P256 sign *********************
Signature generated successfully.
****************** Open Verify service ********************
Verify service open successfully. Verification handle ID: 0xf623f2c7
****************** ECC NIST P256 verify *******************
ECC NIST p256 Signature verified successfully!
****************** Key Delete (ECC NIST P256) *************
Key deleted successfully. Key Pair ID: 0x6ffffffd
****************** Key Generate (ECC Brainpool) ***********
Key generated successfully. Key Pair ID: 0x6ffffffd
****************** ECC Brainpool sign *********************
Signature generated successfully.
****************** ECC Brainpool verify *******************
Brainpool Signature verified successfully!
****************** Key Delete (ECC Brainpool) *************
Key deleted successfully. Key Pair ID: 0x6ffffffd
****************** Key Generate (RSA PKCS1 V1.5) **********
Key generated successfully. Key Pair ID: 0x6ffffffd
****************** RSA PKCS1 V1.5 sign ********************
Signature generated successfully.
****************** RSA PKCS1 V1.5 verify ******************
RSA Signature verified successfully!
****************** Key Delete (RSA PKCS1 V1.5) ************
Key deleted successfully. Key Pair ID: 0x6ffffffd
****************** Key Generate (RSA PSS) *****************
Key generated successfully. Key Pair ID: 0x6ffffffd
****************** RSA PSS sign ***************************
Signature generated successfully.
****************** RSA PSS verify *************************
RSA Signature verified successfully!
****************** Close Verify service *******************
Verify service close successfully.
****************** Close Sign service *********************
Sign service close successfully.
****************** Close cipher service *******************
Cipher service closed successfully.
****************** Close MAC service **********************
MAC service closed successfully.
****************** Key Management Close *******************
Close Key management service successfully.
****************** Close Key Store ************************
Close Key Store successfully.
****************** Close EdgeLock session *****************
Close session successfully.
End of Example with SUCCESS!!
The IDs will be different on every run.