Hardware requirements#
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings#
The FreeRTOS Message Buffers multicore project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the FreeRTOS Message Buffers multicore demo in the terminal window:
FreeRTOS Message Buffers demo starts
Copy CORE1 image to address: 0x303C0000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
FreeRTOS Message Buffers demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.