MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:

RPMsg demo starts

Copy CORE1 image to address: 0x303C0000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101

RPMsg demo ends

Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.