Hardware requirements

  • Mini/Micro USB cable

  • FRDM-K32L2A4S board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo

  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

LPI2C example -- Read Accelerometer Value

Found a FXOS8700 on board , the device address is 0x1e .

The accel values:

status_reg = 0xff , x =    24 , y =   -66 , z =  2119
status_reg = 0xff , x =    24 , y =   -65 , z =  2120
status_reg = 0xff , x =    27 , y =   -68 , z =  2112
status_reg = 0xff , x =    29 , y =   -64 , z =  2114
status_reg = 0xff , x =    21 , y =   -66 , z =  2114
status_reg = 0xff , x =    31 , y =   -69 , z =  2124
status_reg = 0xff , x =    28 , y =   -65 , z =  2117
status_reg = 0xff , x =    28 , y =   -67 , z =  2115
status_reg = 0xff , x =    24 , y =   -64 , z =  2114
status_reg = 0xff , x =    28 , y =   -73 , z =  2115

End of LPI2C example .