Hardware requirements

  • Micro USB cable

  • FRDM-KE16Z board

  • Personal Computer

Board settings

The example requires connection between the trgmux pin and oscilloscope. Connect each of the trgmux output pin with the anode of oscilloscope: J2-3(FRDM-KE16Z board) -> Anode of oscilloscope. Or J1-12(FRDM-KE16Z board) -> Anode of oscilloscope. Or J2-5 (FRDM-KE16Z board) -> Anode of oscilloscope. Or D4-3 (FRDM-KE16Z board) -> Anode of oscilloscope.

GND (FRDM-KE16Z board) -> Cathode of oscilloscope.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the 10KHz PWM on each of the 8 pins.