Hardware requirements
- Micro USB cable 
- FRDM-KE17Z512 board 
- Personal Computer 
Board settings
Connect input signal to J2-11
Prepare the Demo
- Connect a USB cable between the host PC and the MCU-LINK USB port on the target board. 
- Open a serial terminal with the following settings: 
- 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. 
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
PWT example: input signal whose pulse width needs to be measured
Toggled Low overflow
Positive pulse width=16 usec
Negative pulse width=11 usec
Toggled High overflow
Positive pulse width=11 usec
Negative pulse width=17 usec