Hardware requirements#
Type-C USB cable
FRDM-MCXA156 board
Personal Computer
Board settings#
MASTER(LPI2C0) connect to SLAVE(LPI2C3)
LPI2C0 SCL(P0_17,J2-20) --> LPI2C3 SCL(P3_27,J5_5)
LPI2C0 SDA(P0_16,J2-18) --> LPI2C3 SDA(P3_28,J5_6)
Other jumpers keep default configuration.
Prepare the Demo#
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .