Hardware requirements

  • Type-C USB cable

  • FRDM-MCXA166 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of this example in the terminal window:

Ramdisk example.
Format ram disk.
Creating text file.
Writing to text file.
Opening file for read.
Text in file.