MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXA174 board

  • Personal Computer

Board settings#

The example requires 2 sets of boards, each of them is mounted with the base board. To make example work, connections needed to be as follows on each base board:

Board to board connections needed to be as follows:

        Node A           connect to      Node B
Pin Name   Board Location         Pin Name    Board Location
CANH       J14-1                  CANH        J14-1
CANL       J14-2                  CANL        J14-2
GND        J14-4                  GND         J14-4

Also need to short JP7 to disable USB to CAN.

Prepare the Demo#

  1. Connect the type-C USB cable between the PC host and the USB ports on the board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

After connecting the two boards, these instructions display on each terminal window. One board must be chosen as node A and the other board as node B. (Note: Node B should start first) Data is sent continuously between the node A and the node B.

This message displays on the node A terminal:

********* FLEXCAN Interrupt EXAMPLE *********
    Message format: Standard (11 bit id)
    Message buffer 10 used for Rx.
    Message buffer 9 used for Tx.
    Interrupt Mode: Enabled
    Operation Mode: TX and RX --> Normal
*********************************************

Please select local node as A or B:
Note: Node B should start first.
Node:A
Press any key to trigger one-shot transmission

Rx MB ID: 0x123, Rx MB data: 0x0, Time stamp: 24291
Press any key to trigger the next transmission!

Rx MB ID: 0x123, Rx MB data: 0x1, Time stamp: 59183
Press any key to trigger the next transmission!

This message displays on the node B terminal:

********* FLEXCAN Interrupt EXAMPLE ********* Message format: Standard (11 bit id) Message buffer 10 used for Rx. Message buffer 9 used for Tx. Interrupt Mode: Enabled Operation Mode: TX and RX –> Normal


Please select local node as A or B: Note: Node B should start first. Node:B Start to Wait data from Node A

Rx MB ID: 0x321, Rx MB data: 0x0, Time stamp: 16425 Wait Node A to trigger the next transmission!

Rx MB ID: 0x321, Rx MB data: 0x1, Time stamp: 51370 Wait Node A to trigger the next transmission!