Hardware requirements
Type-C USB cable
FRDM-MCXA266 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
Press SW2 to turn on/off a LED.
And you will detect voltage toggle on the RED LED.