Hardware requirements
Type-C USB cable
FRDM-MCXA276 board
LCD-PAR-S035 board
Personal Computer
Board settings
Attach the LCD shield to the FRDM board.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J15.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
If this example runs correctly, the sample GUI is displayed.