MCUXpresso SDK Documentation

Overview#

The lpi2c_edma_b2b_transfer_master example shows how to use lpi2c driver as master to do board to board transfer with EDMA:

In this example, one lpi2c instance as master and another lpi2c instance on the other board as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct. Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXA346 board

  • Personal Computer

Board settings#

MASTER(LPI2C2)                connect to        SLAVE(LPI2C2)
Pin Name    Board Location                      Pin Name    Board Location
SCL         J2 pin 20                           SCL         J2 pin 20
SDA         J2 pin 18                           SDA         J2 pin 18
GND         J2 pin 14                           GND         J2 pin 14

Other jumpers keep default configuration.

Prepare the Demo#

  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The following lines are printed to the serial terminal when the demo program is executed.

LPI2C board2board EDMA example -- Master transfer.
Master will send data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f

Receive sent data from slave :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of LPI2C example .