Hardware requirements
- Type-C USB cable 
- FRDM-MCXC444 board 
- Personal Computer 
Board settings
No special settings are required.
Prepare the Demo
- Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board. 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. 
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM example to simulate a timer
Press any key to start timer!
You will see a "-" or "|" in terminal every 1 second:
-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-