Hardware requirements#
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings#
LPI2C:
MASTER(I2C0) connect to SLAVE(I2C0)
Pin Name Board Location Pin Name Board Location
LPI2C0_SCL J5-5 LPI2C0_SCL J5-5
LPI2C0_SDA J5-6 LPI2C0_SDA J5-6
GND J5-8 GND J5-8
Make sure you have solder bridges SJ1 and SJ2 set to
2-1 for the main core (cm33)
Prepare the Demo#
Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board EDMA example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .