Hardware requirements#
Type-C USB cable
FRDM-MCXN947 Board
Personal Computer
Board settings#
The example requires 2 sets of boards, each of them is mounted with the base board. To make example work, connections needed to be as follows on each base board:
Board to board connections needed to be as follows:
Node A connect to Node B
Pin Name Board Location Pin Name Board Location
CANH J10-1 CANH J10-1
CANL J10-2 CANL J10-2
GND J10-4 GND J10-4
Prepare the Demo#
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
After connecting the two boards, these instructions display on each terminal window. One board must be chosen as node A and the other board as node B. (Note: Node B should start first) Data is sent continuously between the node A and the node B.
This message displays on the node A terminal:
********* FLEXCAN Interrupt EXAMPLE *********
Message format: Standard (11 bit id)
Message buffer 10 used for Rx.
Message buffer 9 used for Tx.
Interrupt Mode: Enabled
Operation Mode: TX and RX --> Normal
*********************************************
Please select local node as A or B:
Note: Node B should start first.
Node:A
Press any key to trigger one-shot transmission
Rx MB ID: 0x123, Rx MB data: 0x0, Time stamp: 24291
Press any key to trigger the next transmission!
Rx MB ID: 0x123, Rx MB data: 0x1, Time stamp: 59183
Press any key to trigger the next transmission!
This message displays on the node B terminal:
********* FLEXCAN Interrupt EXAMPLE ********* Message format: Standard (11 bit id) Message buffer 10 used for Rx. Message buffer 9 used for Tx. Interrupt Mode: Enabled Operation Mode: TX and RX –> Normal
Please select local node as A or B: Note: Node B should start first. Node:B Start to Wait data from Node A
Rx MB ID: 0x321, Rx MB data: 0x0, Time stamp: 16425 Wait Node A to trigger the next transmission!
Rx MB ID: 0x321, Rx MB data: 0x1, Time stamp: 51370 Wait Node A to trigger the next transmission!