Hardware requirements#
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Note: MCUXpresso IDE project default debug console is semihost
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the hello world multicore demo in the terminal window:
Copy Secondary core image to address: 0x2004e000, size: 3280
Starting Secondary core.
Hello World from the Primary Core!
Starting Secondary core.
The secondary core application has been started.
Note: The “Copy Secondary core image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.