Hardware requirements#
Type-C USB cable
FRDM-MCXW23 Board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
DMA hardware trigger example begin.
Destination Buffer:
0 0 0 0
Press SW2 to trigger one shot DMA transfer.
SW2 is pressed.
DMA hardware trigger example finish.
Destination Buffer:
1 2 3 4