Hardware requirements

  • Type-C USB cable

  • FRDM-MCXW72 Board

  • Personal Computer

Board settings

This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.

Prepare the Demo

  1. Connect a USB cable between the host PC and the board J10.

  2. Download the program to the target board.

  3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the eRPC Two Way RPC RTOS demo in the terminal window:

Primary core started
Get number from core1:
Got number: 1
Start normal rpc call example.
RPC call example finished.

Get number from core1:
Got number: 2
Start normal rpc call example.
RPC call example finished.

Get number from core1:
Got number: 3
Start normal rpc call example.
RPC call example finished.
.
.
.