Hardware requirements#
Micro USB cable
FRDM-RW612 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo#
The message about error or success will be output to the terminal.