Hardware requirements
- Micro USB cable 
- FRDM-RW612 board 
- Personal Computer 
Board settings
Prepare the Demo
- Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Launch the debugger in your IDE to begin running the demo. 
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Usart functional interrupt example
Board receives characters then sends them out
Now please input: