Hardware requirements#
Micro USB cable
IMX952-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings#
No special settings are required.
Please note this application can’t support running with Linux BSP!#
Prepare the Demo#
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, you will see the similar information from the terminal shown as below. Detail prints for each channel depends on by the total numbs of chained channels and the order of interrupt flag handler process for each channel.
Starting channel No.0 ...
Starting channel No.1 ...
Starting channel No.2 ...
Starting channel No.3 ...
Channel No.0 interrupt is occurred !
Channel No.0 interrupt is occurred !
Channel No.0 interrupt is occurred !
Channel No.0 interrupt is occurred !
Channel No.0 interrupt is occurred !
Channel No.1 Chained with Channel No.0 interrupt is occurred !
......................................
Channel No.1 Chained with Channel No.0 interrupt is occurred !
......................................
Channel No.1 Chained with Channel No.0 interrupt is occurred !
......................................
Channel No.1 Chained with Channel No.0 interrupt is occurred !
......................................
Channel No.1 Chained with Channel No.0 interrupt is occurred !
Channel No.2 Chained with Channel No.1 interrupt is occurred !
......................................
......................................
Channel No.2 Chained with Channel No.1 interrupt is occurred !
......................................
......................................
Channel No.2 Chained with Channel No.1 interrupt is occurred !
......................................
......................................
Channel No.2 Chained with Channel No.1 interrupt is occurred !
......................................
......................................
Channel No.3 Chained with Channel No.2 interrupt is occurred !
.....................................
.....................................
.....................................