MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • IMX95LP4X-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings#

No special settings are required.

Please note this application can’t support running with Linux BSP!

Prepare the Demo#

  1. Connect 12V~20V power supply and JLink Plus to the board, switch SW4 to power on the board

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, please speak or play a song nearby microphone, then you will see log on the terminal like:

PDM hwvad example started!

Voice detected

Voice detected

...

PDM hwvad example finished!

Note: There is a variable in this example which initial as 50, once voice detected, it will decrease by one until 0, then example finish.