Hardware requirements
Micro USB cable
IMX95LPD5EVK-19 board
J-Link Debug Probe
12V~20V power supply
Personal Computer
LCD SPEC panel
Board settings
For DUAL LVDS panel(19201200), connect MINISAS ports J15 and J16 to panel. For LCD SPEC panel(1280800), connect MINISAS port J15 to MINISAS2LVDS card as LVDS0. J16 to MINISAS2LVDS card for LVDS1. The MINISAS2LVDS card need jumper, please refer to the card datasheet. For LVDS2HDMI card(19201080), connect MINISAS port J16 to panel. For MX9_DSI_OLED MIPI panel(10802340), connect MINISAS port J14 to panel. For MIPI2HDMI card(1920*1080), connect MINISAS port J14 to panel.
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Load the figure binary file by using Jlink command “loadbin xxx.bin 0x80000000” and “loadbin xxx.bin 0x803e8000”(default LCD SPEC panel).
| panel name | buffer address 1 | buffer address 2 |
| DUAL LVDS | 0x80000000 | 0x808ca000 |
| LCD SPEC | 0x80000000 | 0x803e8000 |
| MX9_DSI_OLED | 0x80000000 | 0x809a3f80 |
| MIPI2HDMI | 0x80000000 | 0x807e9000 |
| LVDS2HDMI | 0x80000000 | 0x807e9000 |
Steps to configure the panels
Default panel is LCD SPEC panel, default port is DPU_DI_LVDS, default setting for APP_DISPLAY_EXTERNAL_CONVERTOR is disabled Tips: The APP_DISPLAY_EXTERNAL_CONVERTOR can be set as 1 when you are using MIPI2HDMI card(ADV7535) or LVDS2HDMI card(IT6263) only. When Kconfig is used
Below setting is for kconfig, you can fix below settings in dpu/figure_display/cm7/prj.conf For default LCD_SPEC panel, you do not need to change anything. For DUAL LVDS panel(19201200): CONFIG_MCUX_PRJSEG_module.board.display_support.LVDS_DUAL_PANEL=y CONFIG_MCUX_PRJSEG_module.board.display_support.LDB_DUAL_PANEL_ENABLE=y For LVDS2HDMI card(19201080): CONFIG_APP_DISPLAY_EXTERNAL_CONVERTOR=y CONFIG_MCUX_PRJSEG_module.board.display_support.LVDS2HDMI=y For MIPI DSI panel(10802340): CONFIG_MCUX_PRJSEG_module.board.display_support.DPU_DI_MIPI=y CONFIG_MCUX_PRJSEG_module.board.display_support.MX9_DSI_OLED=y For MIPI2HDMI card(19201080): CONFIG_MCUX_PRJSEG_module.board.display_support.DPU_DI_MIPI=y CONFIG_APP_DISPLAY_EXTERNAL_CONVERTOR=y CONFIG_MCUX_PRJSEG_module.board.display_support.MIPI2HDMI=y When package is used
Below setting is for mcux_config.h. Setting DEMO_PANEL to LVDS_DUAL_PANEL to DUAL LVDS panel(19201200). You also need to set LDB_DUAL_PANEL to 1. Setting DEMO_PANEL to LVDS2HDMI to use LVDS2HDMI card(19201080), you need to set APP_DISPLAY_EXTERNAL_CONVERTOR to 1. Setting DEMO_PANEL to MX9_DSI_OLED to use MIPI DSI panel(10802340), you also need to set DPU_EXAMPLE_DI to DPU_DI_MIPI. Setting DEMO_PANEL to MIPI2HDMI to use MIPI2HDMI card(19201080), you need to set DPU_EXAMPLE_DI to DPU_DI_MIPI. And you also need to set APP_DISPLAY_EXTERNAL_CONVERTOR to 1. For default LCD_SPEC panel, you do not need to change anything.
Running the demo
When the example runs successfully, you can see the expected figure shown in screen.