Hardware requirements
Micro USB cable
IMX95VERDIN-EVK Board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board.
Connect a USB cable between the host PC and the Debug port on the board (Refer “Getting Started with MCUXpresso SDK for IMX95VERDIN-EVK.pdf” for debug port information).
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board (Please refer “Getting Started with MCUXpresso SDK for IMX95VERDIN-EVK.pdf” for how to run different targets).
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
EDMA memory to memory transfer example begin.
Destination Buffer:
0 0 0 0
EDMA memory to memory transfer example finish.
Destination Buffer:
1 2 3 4